Skip to main content

Daikin adds new Refrigerant Leak Detection capability to remote monitoring services for chiller

14/10/2021

Daikin has announced the launch of a new, smart Refrigeration Leak Detection feature to assist chiller equipment and plant users with safety management and F-Gas compliance.

The technology behind the new function is based on a unique new software algorithm developed by Daikin which uses historical data to raise an alarm in the event of a potential leakage and to report on the frequency of occurrences over time, allowing users to decide whether action is required.

The new algorithm detects even slow gas leakages over an extended load range, starting at 33% of unit load compared to 50% for other applications on the market, while referencing data from one month up to the 12 months previously.

Improved performance reliability

Detection of small leaks at an early stage allows Daikin engineers to intervene promptly, minimising discomfort to the customer and conserving valuable refrigerant.

Leading the market

The new Refrigerant Leakage Detection service is now available as part of the Daikin on Site (DoS) cloud-based remote monitoring and control system. Setting new performance standards, the new Refrigerant Leak Detection service is distinguished by convenience and cost-effectiveness, as well as by the intelligent technology behind it.

Monitoring through the existing cloud removes the need for additional refrigerant leakage detection sensors and a local controller, helping to offset initial system purchase costs. The machine learning technology incorporated in the DoS cloud services enables improved detection rates of 15% for leakages, surpassing current market performance. Faster leak identification and repair prevents the release of harmful refrigerants into the atmosphere, helping users to minimize their environmental impact.

More options

The Refrigerant Leak Detection function can also be suppled bundled as part of a maintenance contract for users who choose to outsource monitoring and management services, where the service engineer receives an alarm at the time of leakage detection, analyses the situation remotely and on site, and quotes necessary repair measures as necessary.

Daikin plans to extend its refrigerant leak detection capabilities soon, with the introduction of a comprehensive refrigerant management service to assist Daikin equipment users with F Gas compliance through a one stop shop that includes the management of the amount of refrigerant and fulfilment of inspection requirements.

Working with you to improve the environment

The new Refrigerant Leak Detection Service is the latest in a series of advances, driven by a continuous product development programme which is focused on innovation, performance and energy efficiency.

 

Available now: To add the new Refrigerant Leak Detection service to your subscription, contact your local Daikin office.

About Daikin Europe N.V.

Daikin Europe N.V. is a major European producer of air conditioners, heat pumps and refrigeration equipment, with approximately 5,500 employees throughout Europe and 10 major manufacturing facilities based in Belgium, the Czech Republic, Germany, Italy, Turkey and the UK.

Globally, Daikin is renowned for its pioneering approach to product development and the unrivalled quality and versatility of its integrated solutions. With more than 90 years’ experience in the design and manufacture of heating and cooling technologies, Daikin is a market leader in heat pump technology. Daikin VRV and Daikin Altherma are the most sold heat pump systems in Europe, with over 500,000 systems delivered to date.

Related articles

Need help?

Need Help?

Find more information

Need help?