Daikin has announced the release of an updated version of its FAA-B wall-mounted indoor unit, designed for use with the company’s full line-up of Sky Air A-series R-32 heat pumps.
For the retail sector, contributing to reducing the industry’s environmental impact is key, with the decarbonization of building premises being one of the primary goals. The elegant appearance and advanced technology of Daikin’s new wall mounted unit offers an appealing package that is easy to install, intuitive to control and makes energy-saving heat pump technology accessible to all types of retail outlets to replace traditional boiler systems.
Versatile design options
The new unit gives installers and designers optimum flexibility in design and location when connected to the Sky Air Alpha-series outdoor unit. The combination offers long piping lengths up to 85 metres and a wide operation range down to -20°C. An optional sound enclosure can reduce outdoor sound power by up to -10dB(A), allowing the combination to be installed in any location, even city centres and mixed urban areas subject to strict noise regulation.
World class performance
Through connection to the complete range of Sky Air A-Series outdoor units, the widest R-32 refrigerant portfolio available in the market, the system offers a future-proof lower GWP solution that greatly reduces environmental impact compared to traditional systems using R-410A refrigerant.
Total Control
With Daikin’s optional smart eco-control Onecta app, optimising the indoor environment is easy. Online control and scheduling helps maximise energy efficiency, while assuring the comfort of staff and shoppers.
The new model is available from early 2022 onwards. For more information visit:
https://www.daikin.eu/en_us/products/faa-b.html
About Daikin Europe N.V.
Daikin Europe N.V. is a major European producer of air conditioners, heat pumps and refrigeration equipment, with 10,000 people employed throughout Europe and fourteen major manufacturing facilities based in Belgium, the Czech Republic, Germany, Italy, Turkey, Austria and the UK.
Building a sustainable legacy together
Air is everywhere and is essential to our lives. At Daikin, ensuring the purity of air we breathe in indoor environments, both now and for the future, is our greatest concern.
Daikin’s mission is to deliver healthier indoor air while minimising environmental footprint. Inspired by a dedication to achieve Net Zero CO2 emissions by 2050, Daikin solutions provide safe, healthy and comfortable spaces throughout the building life cycle using world-leading technology.
Building long term relationships, we continue to work with customers and partners to protect the health and well-being of every individual.