Skip to main content

Hotel Santos Porta Fira

Barcelona, Spain

Porta Fira is a unique, skyscraper hotel totalling 26-storeys and 113m high. A landmark near the Fira, a prominent exhibition space in Barcelona, this 4-star hotel beat 300 other skyscrapers around the world to win the Emporis Skyscraper Award in 2010.

The Santos Group, the organisation in charge of building Porta Fira, selected Daikin as a trusted partner to deliver a unique, reliable and energy-efficient climate control system for the building.

Unique portfolio provides the ideal climate

For Porta Fira, we delivered a custom solution that uses a mix of air-to-air heat pumps and air-to-water chillers. In each hotel room, we installed VRV heat recovery units to ensure guests can individually control the climate. The heat recovery system also provides the highest energy efficiency by taking excess heat from areas on the south side of the building and moving it to the north side. Large spaces including meeting rooms, the restaurant and lobby, use a Daikin chiller system to provide a cool room temperature during warm summer months.

Year-round comfort guaranteed

We set up our Intelligent Network system to monitor Porta Fira's air conditioning system 24/7. This proactive system is an asset because it goes beyond regular maintenance, as it detects the likelihood of issues to happen, to prevent potential breakdowns.

From the moment the system deviates outside standard parameters, an evaluation occurs, followed by immediate support by a team of engineers and experts if necessary. Through this process, the hotel ensures the ideal climate for guests while extending the life of the system.

Solution at a glance

  • 74 VRV heat pump and heat recovery units
  • Intelligent touch manager central controller
  • 664 concealed ceiling indoor units
  • 2 air-cooled chillers

Learn more

Our other cases

  • Hotel Santos Porta Fira

    The Santos Group, the organisation in charge of building Porta Fira, selected Daikin as a trusted partner to deliver a unique, reliable and energy-efficient climate control system for the building.
  • Torre Serenissima

    Equipped with an outdated R-22 refrigerant system, we gave the Torre Serenissima a full upgrade to deliver more energy efficiency and comfort.
  • Venetian Arsenal

    An innovative climate control system that taps into the natural energy of the Venetian Lagoon is delivering high levels of comfort and energy efficiencies while preserving an historic industrial building in the heart of Venice.
  • Crystal Tower

    To help Crystal Tower maximise its energy efficiency, we planned to combine the power of air-cooled VRV, water-cooled VRV and chillers to deliver an all-in-one climate control solution.

Need help?

Need Help?

Find more information

Need help?